Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an SC2040M200PF, Series M01?

Article available in these languages: Spanish

Issue:
Current design repair parts

Product Line:
CSED Combination Service Entrance Devices

Resolution:
The repair part numbers for the SC2040M200PF, Series M01, are shown in the below list. These are the ONLY parts that can be field replaced. Other parts are not replaceable.
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW
Meter Cover Assembly - 4053442852
Meter Cover Mounting Screw - 4020513001K (contains 10 screws, but only 1 is required)
Branch Wiring Gutter Cover (Below Meter Cover) - 4056178101
Branch Wiring Gutter Cover Mounting Screw - 4020513001K (contains 10 screws, but only 1 is required)
Utility Pullbox Cover - 4056181150 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - EAV68546 (includes the hinges)
Load Center Cover Mounting Screws - 2142217101 (2 required)
Dead Front Interior Trim - EAV67735 (DOES NOT INCLUDE ANY LABELS)
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws, but only 2 are required)
Load Center Interior - MTR10000 (main breaker and large branch neutral lugs not included)
Load Center Interior Mounting Screw - 4020510001 (2 required)
Main Breaker - QOM2200VH
Mounting screw for Main Breaker - 4020511201 (1 required, BUT it comes with the main breaker)
Keps nut for mounting Main Breaker to bus bar - 2342702001 (2 required)
Meter Base - 4054102503 (Base ONLY - does not include line and load phase jaws, see below)
Meter Base Mounting Screw - 2142717200 (1 required)
Meter Jaw - 7329746450 (4 required, includes blade guides)
Meter Jaw Mounting Keps Nut - 2342702001(1 required per Meter Jaw)
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Left Line Side Phase Lug - 4025116051
Left Line Side Phase Lugs Mounting Bolt - 2271020242
Left Line Side Phase Lugs Mounting Keps Nut - 2342702001
Large Branch Neutral Lugs - LK70AN (the device comes with 3 lugs as standard from the factory)
Right Line Side Phase Lug and Line Side Neutral Lug are NOT field repairable.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings