Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the deadfront for the NQSFB4HJ when only using one subfeed breaker?
Issue:
What is the part number for the deadfront for the NQSFB4HJ when only using one subfeed breaker?

Product Line:
NQ panelboards sold and supported in the USA.

Environment:
Maintenance/installation

Cause:
Requirement to blank off one side when only using one subfeed breaker in the twin unit mounting pan.

Resolution:
Use part number 80114-397-01 for one side.

Note: 80114-397-01  is an Interplant part number. Please contact your Local Square D Sales Representative for more information.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings