Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What comes with the NFNL1 and NFNL2 neutral kits?
Issue:
What comes with the NFNL1 and NFNL2 neutral kits?

Product Line:
NF Panelboards

Environment:
NFN1CU, NFN2CU, NFN6CU (Copper Neutrals) and NFNL1, NFNL2, and NFNL4 (200% Neutral)

Cause:
Needs to know what is included in the kit.

Resolution:
The NFNL1 and NFNL2 kit contains (1) neutral assembly and (4) 10-32 x 5/16-inch tapping screws.
Please refer to the attached instruction bulletin 80043-754-02 for installation.

Tools required but NOT included is a  #2 Square-head Robertson driver.

Schneider Electric USA

Attachment(s)
NFNL1 and NFNL2 80043-754-02.pdf [2.1 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings