Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for ZCKJ921H4
Issue:
What is the replacement for ZCKJ921H4

Product Line:
XCKJ

Environment:
Limit Switches

Resolution:
Order the standard device with metric fitting, ZCKJ921, and add the adapter to 1/2 in NPT, which is DE9RA1012.  Both of these parts are system recognized and together can substitute for the ZCKJ921H4.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings