Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the NQ and NF panel covers come with a door and lock?
Issue:
Do the NQ and NF covers come standard with a lockable door?

Product Line:
Panelboards

Environment:
NQ and NF

Cause:
Customer wants a door on his panelboard.

Resolution:
Yes, all NQ and NF Mono-Flat covers comes standard with a door and lock. This is also true for for the hinged Trim covers as well

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings