Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
For the EX45T3H, what is the part number for the wall mounting bracket?
Issue:
What is the part number for the wall mounting bracket ​for the EX45T3H transformers?

Product Line:
General Dry Type 600 Volts and Below

Environment:
Energy Efficient,  Three Phase Transformers, 18K enclosures, 20K enclosures, wall mounting bracket.

Cause:
Wants to hang transformer on wall.

Resolution:
The EX45T3H Transformer wall mounting bracket is part umber 7400WMB18K20K. This applies to both the 18K and 20K EX, 3 phase enclosures.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings