Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you ship a can or panel enclosure, ahead or from stock, on a factory assembled panel that states ship completely assembled?
Issue:
Can you ship a can or panel enclosure,  ahead or from stock, on a factory assembled panel that states ship completely assembled?

Product Line:
Panel boards

Environment:
All panels, I-line, NF, NQ, QMB

Cause:
Product needed ASAP, installation

Resolution:
No. It is not supported nor recommended to ship cans ahead. Panels that are designated and specified to ship completely assembled are due to a few issues.
1. Power supplies and CT's required are shipped complete and wired from the factory.
2. Panels that are supplied with the 600A L frame mains are two heavy so the can is shipped with the interior to protect the interior from damage during shipping.
3. Split bus panels require special construction and again the weight of the panel and the two interiors are a factor.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings