Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will an NF panel work on DC applications?
Issue:
Can an NF panelboard be used on DC application?

Product Line:
NF panelboards

Environment:
Panelboards.

Cause:
Panel needed for a DC application.

Resolution:
The NF panel is not designed for DC applications. If a DC application is needed the NQ and I-Line panelboards may be used.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings