Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: What is Shielded Solid Insulated Switchgear (2SIS)?
Issue:
What is Shielded Solid Insulated Switchgear (2SIS)?

Product Line:
MV switchgear

Environment:
Premset Product line

Cause:
Product features

Resolution:
It is a new generation of medium voltage switchgear that offers a modular design and a reduced footprint as compared to Air Insulated or Gas Insulated switchgear. Each current carrying conductor is individually coated in a molded EPDM insulating epoxy. Additionally, a conductive ground layer is formed on top of the insulating layer to make a ground potential shielded layer surrounding each phase. This garners multiple benefits including, small footprint, longer switchgear life, reduced maintenance, and better environmental protection.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings