Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does 2SIS switchgear reduce Arc Flash requirements?

Issue:
2SIS switchgear reduced Arc Flash requirements

Product Line:
MV Switchgear

Environment:
Premset Switchgear

Cause:
Product features

Resolution:
It reduces the risks of an Arc Flash, but it does not reduce the hazard. This means the probability of an arc flash is reduced, but 2SIS does not address the available incident energy on the electrical network.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings