Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How tall is the 2SIS switchgear?
Issue:
height of 2SIS switchgear

Product Line:
MV Switchgear

Environment:
Premset Switchgear

Cause:
Product features

Resolution:
It has a minimum height of 65". The modular addition of taller LV boxes or cable pulling boxes can increase the height in some applications.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings