Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the largest sub feed breaker that can be added to a NQ panel?
Issue:
​What is the highest ampacity SFB that can be added to a NQ panel?

Product Line:
Panelboard

Environment:
NQ panelboard, subfeed breaker

Cause:
Application and product features

Resolution:
The largest subfeed breaker that can be added to the NQ panel is 225A Max for N1 and 150A Max for N3R, N12, N3R/12

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings