Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are EZM main devices available with an energy reduction maintenance switch (ERMS)?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
EZM Metering

Resolution:
See the table below for all the EZM main device catalog numbers with an ERMS.
Also, see attached a handout introducing the EZM main devices with an ERMS.
ERMS table

Schneider Electric USA

Attachment(s)
2014 NEC Arc Energy Reduction in EZM Main Devices.pdf [117.54 KB]
EZM Mains with ERMS Final Handout 4141HO1602.pdf [162.03 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings