Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an RC12L200C, series M02?
Issue:
Current design repair parts

Product Line:
Combination Service Entrance Device

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 7329463951 (includes latch)
Load Center Cover - 7329463952 (includes hinges)
Load Center Cover Mounting Screws - 2159417121 (2 required)
Dead Front Interior Trim - 7329463914
Dead Front Interior Trim Mounting Screws - 4020513001K (contains 10 screws; only 2 are required)
Load Center Interior - 7329463960
Load Center Interior Mounting Screw - 2153217161 (1 required)
Load Center Interior mounting brackets - 7329463916 (2 required)
Mounting screws for above Load Center Interior brackets - 2142217101 (1 per bracket)
Load Center Interior Mounting Pan - 7329463919
Mounting screws for the Interior Mounting Pan  - 2142217101 (4 required)
Meter Base Assembly - 7329463950 (includes phenolic meter base, line side lug assembly, and line side meter jaws with jaw blade guides)
Mounting screws for the Meter base assembly - 2149020100 ( 3 required)
Load side Meter Socket Jaw with Blade Guide - 7329746450 (2 required for the load side of the meter socket)
Load side Meter Jaw Mounting Keps Nuts - 2342702001 (1 per meter jaw)
Meter Jaw Blade Guide - 4052761901
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings