Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the Impedance (%IZ) for the EE15T3H transformer?
Issue:
What is the (%IZ)  for the EE15T3H transformer?

Product Line:
LV Transformers, 600 Volts and Below, Energy Efficient

Environment:
EE15T3H, 3 phase, 60 Hz,480V Delta primary, 208Y/120Vac secondary, UL Listed

Cause:
Impedance of Transformers is information often required by specifications, and for calculations for Average Interrupting Current, Voltage Regulation, and other factors.

Resolution:
The impedance for the EE15T3H is 5.1 per the Energy Efficient Transformers Technical Data Bulletin 7400DB0702R07/09, page 4.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings