Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement covers for a EE112T3HBISCUNLP and all other EE type transformers with the 22D style enclosure?
Issue:
What is the replacement covers for a EE112T3HBISCUNLP and all other EE type transformers with the 22D style enclosure?

Product Line:
LV Transformers, 600V and Below

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Cover was damaged they need a replacement.

Resolution:
The enclosure  for the EE112T3HBISCUNLP is a 22D which has the following replacements:
Enclosure Parts
Top cover 4310189001
Front 4310189102 (When replacing a front panel, specify the transformer part number and ?with nameplate and labels? on the order.)
Rear 4310189102
Sides (ends) 4310189201
Base 4310189550

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings