Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the SXRM X-ray receptacle modules come in surface and flush mounts?
Issue:
SXRM X-ray receptacle modules come in surface and flush mounts

Product Line:
medical products X-ray modules

Environment:
SXRM

Cause:
product features

Resolution:
The SXRM X-ray panels or modules are available in both surface and flush mount. The part numbers in the catalog are all for flush mounting. For surface mounting, add an S to the end of the box catalog number SB120804 to become SB120804S and contact your local distributor or sales office for special pricing for a surface mount cover as the surface covers are not currently system recognized.

Schneider Electric USA

Attachment(s)
4800CT1201 2015 X-ray Mod.pdf [54.81 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings