Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for the EZM1600FST and EZM1800FST main devices?
Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Resolution:
The molded case switch used in EZM1600FST and EZM1800FST is the PowerPact M frame and the standard lug is AL800M23K and will accept as standard:
(3) 3/0 - 500 kcmil Al/Cu wires per phase and the main neutral on these devices will accept as standard (4) 3/0 - 500 kcmil Al/Cu wires

Alternate lugs for the molded case switches used in the above catalog numbers:
1) lug kit AL1200P24K will accept (4) 3/0 - 500 kcmil Al/Cu wires per phase (1 lug per kit)
2) lug kit AL800P6K will accept (2) 3/0 - 600 kcmil Al/Cu wires per phase (3 lugs per kit)
3) lut kit AL800P7K will accept (2) 3/0 - 600 kcmil Al/Cu wires (750 kcmil compact Al wires) per phase (3 lugs per kit)

Alternate lugs for the main neutral used in the above catalog numbers:
1) lug kit MMLK250 will accept as standard (1) 1/0 - 600 kcmil OR (2) 1/0 - 250 kcmil Al/Cu wires per lug. Kit includes (3) 2 barrel lugs and neutral will accommodate ONLY 2 lugs.

See drawing for further reference: PWFDS-SYRS-0092

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings