Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for the EZM1600GCBE/JCBE and the EZM1800GCBE/JCBE main devices?
Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Resolution:
The EZM1600GCBE, EZM1600JCBE, EZM1800GCBE, and EZM1800JCBE are all designed to meet the west coast EUSERC utilities requirements and do not come standard with lugs from the factory, but contain lug landing pads to meet the EUSERC requirements. Each lug landing pad on ALL of these catalog numbers will ONLY accommodate (2) lugs per pad. This means these EZM main devices will ONLY accommodate (2) wires per phase/neutral. See attached CAD drawing showing the part numbers of the lugs and the maximum wire size the lugs will accept.

Schneider Electric USA

Attachment(s)
EZM1600_1800_GCBE_JCBE dwg #PWFDS-SYRS-0103.pdf [159.94 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings