Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for the EZM1600GCBT/JCBT and the EZM1800GCBT/JCBT main devices?

Product Line:
EZM Metering

Resolution:
The main breaker used in EZM1600GCBT, EZM1600JCBT, EZM1800GCBT, and EZM1800JCBT is the PowerPacT M-Frame and the standard lug is AL800M23K and will accept as standard:
(3) 3/0-500 kcmil Al/Cu wires per phase (or per pole of the breaker) and the main neutral on these devices will accept as standard (4) 3/0-500 kcmil Al/Cu wires (See the below attached CAD drawing).


Alternate lugs for main breakers used in the above catalog numbers:
1) Lug kit AL1200P24K will accept (4) 3/0-500 kcmil Al/Cu wires (1 lug per kit)
2) Lug kit AL800P6k will accept (2) 3/0 - 600 kcmil Al/Cu wires (3 lugs per kit)
3) Lut kit AL800P7K will accept (2) 3/0 - 750 kcmil (BUT the 750 kcmil wire MUST be compact aluminum wire ONLY) (3 lugs per kit)

Alternate lugs for the main neutral used in the above catalog numbers:
1) Lug kit MMLK250 will accept as standard (1) 1/0-600 kcmil OR (2) 1/0-250 kcmil Al/Cu wires PER lug. Kit includes (3) 2-barrel lugs and neutral will accommodate ONLY 2 lugs.

Schneider Electric USA

Attachment(s)
EZM1600_1800_GCBT_JCBT dwg #PWFDS-SYRS-0099.pdf [156.96 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings