Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal lug data for the EZM11000GCBU/JCBU and EZM11200GCBU/JCBU main devices?
Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Resolution:
The main breaker used in EZM11000GCBU, EZM11000JCBU, EZM11200GCBU, and EZM11200JCBU is the PowerPacT P frame and the standard lug is AL1200P25K and will accept as standard:
(4) 3/0 - 500 kcmil Al/Cu wires per phase and the main neutral on these devices will accept as standard (4) 3/0 - 500 kcmil Al/Cu wires (see the below attached CAD drawing)

Alternate lugs for the main breakers used in the above catalog numbers:
1) lug kit AL1200P6KU will accept (3) 350 - 600 kcmil Al/Cu wires (3 lugs per kit)
2) lug kit AL1200P7KU will accept (3) 3/0 - 750 kcmil (BUT the 750 kcmil wire MUST be compact aluminum wire ONLY) (3 lugs per kit)

Alternate lugs for the main neutral used in the above catalog numbers:
1) lug kit MMLK250 will accept as standard (1) 1/0 - 600 kcmil OR (2) 1/0 - 250 kcmil Al/Cu wires PER lug; kit includes (3) 2 barrel lugs and neutral will accommodate ONLY 2 lugs.

Additional alternate lugs can be used on these catalog numbers, but will REQUIRE the use of a lug landing kit, EZM1200ULL. See attached CAD drawing showing a table of alternate lugs for use with this kit and a visual and instructions for this kit.

Schneider Electric USA

Attachment(s)
EZM11000_11200_GCBU_JCBU dwg #PWFDS-SYRS-0034.pdf [106.73 KB]
EZM1200ULL Instruction Sheet 73293-777-01 w_visual.pdf [1.66 MB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings