Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
NQOD3225Q2MB: Can a shunt trip be added to the Q2 main breaker?
Issue:
Add a shunt trip to the Q2 main breaker

Product Line:
Panelboard Main breaker

Environment:
NQOD panel with Q2 main breaker

Cause:
Adding accessories to the main

Resolution:
No. The Q2 and QB, QD, and QG frame breakers will not accept accessories. The main breaker kits for the NQOD panels are obsolete and no longer available, with no replacement. The current style main breaker kits do not fit the NQOD panel so the main breaker cannot be replaced. This goes for all NQOD panels rated 250A and below. A new panel will be required.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings