Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the minimum clearance required from the ceiling to the top of the EX Transformers?
Issue:
What is the minimum clearance required from the ceiling to the top of the EX and EXN Transformers?

Product Line:
EX and EXN Transformers, General Purpose Dry Type 600 Volts and Below

Environment:
Installation

Cause:
Location Clarification for mounting

Cause:
Customer needs to know how close to the ceiling they may mount an EX or EXN Transformer.

Resolution:
Suggested minimum clearance from top of a ventilated Transformer to heat-sensitive equipment mounted directly above it or the ceiling above it is 36". This allows proper evacuation of the heated air from the core/coil. The surface of a ceiling above the Transformer should be constructed with the knowledge that air up to 50°C above ambient can be emitted from the Transformer vent openings. The installer should also monitor the temperature of the upper unit to insure that it is not overheating, making sure that the top unit’s ambient temperature does not exceed the 30C average with the BTUs rising up from the lower unit.  Also, it is good practice to install a metal barrier or baffle between vertically mounted Transformers to prevent heat from the lower unit from rising and heating the upper unit. This applies to EE, EX and EXN series Transformers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings