Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is it possible to get a single phase transformer rated for 480V to 120/208V?
Issue:
Is a single phase transformer rated for 480V to 120/208V available?

Product Line:
Low Voltage Transformers

Environment:
Single phase transformers

Cause:
Possible voltages for single phase transformers

Resolution:
No, a 208 voltage on the secondary side applies to 3 phase transformers only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings