Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Why are DC voltages from neutral to ground, 80-100+ VDC, being measured in a NQ panel with SPD's ?
Issue:
DC voltages from neutral to ground, 80-100+ VDC, are measured in a NQ panel with SPD's

Product Line:
Integral TVSS

Environment:
Installation

Cause:
Clarification

Resolution:
When Service Entrance Wye voltage panels are used with Surgelogic TVSS's and the Neutral Bonding strap is loose/ missing, it will cause the SPD to generate a DC voltage between ground and neutral . Remedy for this occurance would be to tighten bonding strap, or install neutral bonding strap if missing. This will allow a clear path for monitoring of the SPD. Situation with open neutral to ground is high resistance due to loose/ missing connection to ground, which is causing DC voltage to be seen.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings