Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the paint process is for the MH-WP boxes?
Issue:
Process for painting MH-WP boxes.

Product Line:
Panelboards

Environment:
Manufacturing process

Cause:
What is the paint process?

Resolution:
Paint specifications are attached. We use an Ecoat cathodic paint system with 9 stages of cleaning.
When we paint enclosures a special color we run the enclosure through our standard gray paint system before painting the special color with powder coat over the gray.
N3R boxes are not available unpainted.

Schneider Electric USA

Attachment(s)
Paint Specifications PTO200.doc [125.5 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings