Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement catalog number for the back panel and top panel for a EX112T3H transformer?
Issue:
What are the repair parts for the Enclosure of the EX112T3H transformer?

Product Line:
Transformers

Environment:
EX Three Phase General Purpose Dry Type 600 Volts and Below

Cause:
Transformer enclosure was damaged, replacement enclosure needed.

Resolution:
The EX112T3H has the 21K enclosure. The Enclosure replacement parts are as follows ( refer to EX Low Voltage Transformer, Catalog 7400CT1501).
Top Cover: NHA52142
Side Panel: NHA52134
Front panel with labels: NHA52143
Rear Cover: NHA52144
Rear Shield: NHA52145
Core Leg: NHA52133
Base Assembly: NHA52091
When ordering front cover with labels, Catalog No., Series No., and Date Code in Engineering Notes must be supplied.  (see Figure 4 found on page 5 of the 7400CT1501 Catalog for location information on Nameplate - attached). Serial number may also be obtained from Core and Coils.

Schneider Electric USA

Attachment(s)
7400CT1501 Nameplate Sampe Fig 4.pdf [104.3 KB]
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings