Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the 8940SS Pump Panels, UL508 listed?
Issue:
Are the Class 8940 Type SS pump panels UL580 listed?

Product Line:
Class 8940 Pump Panels

Environment:
Motor Starters

Cause:
Product Characteristics

Resolution:
UL 508 is a broad standard that covers industrial control equipment. Yes, all Motor Starters are listed for the UL508.  Pump Panels are Motor Starters, they are UL listed and marked "Suitable for Use As Service Equipment".

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings