Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can cables exit the sides of Speed D boards?
Issue:
Exit Speed D boards from the sides

Product Line:
Switchboards

Environment:
Speed D Switchboard

Cause:
Application, product features and wiring

Resolution:
No, it is not supported. A load side wire way section is advised, as there is not enough room in the main switchboard to exit the side.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings