Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you add the series E-4 subfeed breaker Kits to the older series Speed D boards?
Issue:
The Series E-4 subfeed breaker Kits can be used on older series Speed D Boards

Product Line:
Switchboards

Environment:
Speed D switchboards

Resolution:
No, the breakers have changed to a power pact breaker, and therefore have different connectors, which will not work with the older Speed-D switchboards.
We do not have an adapter available either. They may have to replace the switchboard if they need to add or replace the old style KAL, KHL, KAP, or KHP breakers.
FAL breakers are still available for replacing a breaker only but not the breaker kit.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings