Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
When is it recommended to have external temperature control for the storage of Panelboards?
Issue:
Ambient temperature ranges suggested for the storage of Panelboards

Product Line:
Panelboards

Environment:
Storage

Cause:
Condensation / Overheating

Resolution:
The Panelboards should be stored in an ambient temperature of 10 - 40 DEG Celsius, or 50 - 104 DEG Fahrenheit.

Consequently any temperature below 10 DEG C/50 DEG F will dictate the need for external/ internal heating , ie. strip heaters with Thermostat.
Condensation can result and cause damage to the electrical carrying parts of the interior if this is not done.

Any temperature above 40 DEG C/104 DEG F,  would require the equipment to be placed into a temperature controlled space that will ensure the ambient temperature does not exceed this temperature limit.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings