Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do we have an OSHPD sticker or label for EX, EXN, MPZ and EE Transformers and Mini Power Zones?
Issue:
OSHPD label for EX,  MPZ and EE  transformers and minipowerzones

Product Line:
Transformers and MPZ/B
Environment:
EX transformers, EE, and MPZ/B

Cause:
label required

Resolution:

As of 04/20/2016 - California hospitals and medical facilities require a label contained in kit.
Below are the label part numbers that are also required for the various transformer or minipowerzones.

7400CAOSHPDK for EX transformers in Type K enclosure, pad or floor mounted.
7400CAOSHPDM for EXN transformers in Type M enclosure.
7400CAOSHPDKO for EX transformers in Type K enclosure mounted on wall mounting brackets
7400CAOSHPDJ for EX transformers in Type J enclosure, pad or floor mounted.
7400CAOSHPDDH for EE transformers in Types D & H enclosures
7400CAOSHPDABC for sealed resin encapsulated transformers and
7400CAOSHPDMPZB for MPZB MiniPower Zones.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings