Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is it possible to increase the depth of a MH-WP panelboard enclosure?
Issue:
Increase the depth of a MH-WP for the NQ and NF panels

Product Line:
Panelboards

Environment:
NQ and NF

Cause:
Deeper box required

Resolution:
The N3R or MH-WP enclosures for the NF and the NQ panels, are available in 8" and 12" deep enclosures unless the standard panel is already 9" deep due to a high ampere rating or main breaker.
To obtain pricing refer to the 176 pricing guide for the price adder, in product selectors select special pricing to add the price and add the description of  8" or 12" deep enclosure depending on which one is required.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings