Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum charge rate for a Conext SW4024?
Issue:
What is the max charge rate for a Conext SW4024 and can I set it up beyond that point.

Product Line:
Conext SW4024, Conext SW series

Environment:
Maximum charge rate parameters

Cause:
Technicians and customers would like to know the maximum charge rate for their inverter

Resolution:
The specifications are outlined in the installation and operation manual in the Electrical specifications, which can be seen here below.  For a Conext SW 2524, the maximum output charge current is 65 Amps.



Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings