Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the optimal voltages to utilize the maximum power point tracking of the MPPT80-600?
Issue:
Voltage parameters for optimum charging

Product Line:
MPPT80-600

Environment:
Installations where renewable energy (Solar) and an XWMPPT80-600 are used.

Cause:
What are the specifications for input Voltages to achieve the maximum point tracking of the charge controller

Resolution:
The minimum operating voltage for the MPPT80-600 is 195V, however to achieve the maximum power point tracking, it is best to have the voltage between 230-510 Volts.  The controller will still function beyond these ranges but it is best to keep them in this range to account for temperature and efficiency.

:



Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings