Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
The XW6848 unit keeps cycling between load shave and AC passthrough and it doesn't remain in one state?

Issue:

XW6848 inverter/charger is repeatedly cycling between AC Passthrough and Load Shave mode.

Product Line:

• XW6848
• XW5548
• XW6048
• XW4548
• XW4024

Environment:

Installations using the XW hybrid inverter/charger.

Cause:

The inverter is switching between Load Shave and AC Passthrough because the battery voltage is fluctuating around the Load Shave exit threshold.

The XW uses the following logic:

Load Shave Exit Voltage = Recharge Volts + 0.5 V

If the battery voltage repeatedly rises above and falls below this threshold, the inverter will continuously alternate between:

Load Shave Mode →
AC Passthrough Mode →
back into Load Shave Mode

This creates the cycling behavior the user observes.

Diagram Reference:

Load Shave Mode

Resolution:

Adjust the Recharge Volts setting so the battery voltage does not hover near Recharge Volts + 0.5 V.
OR ensure that renewable energy (solar, etc.) can maintain the battery voltage above the Load Shave exit threshold, preventing the mode from oscillating.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings