Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are all the possible ways I can stop my generator using the XW AGS?
Issue:
What are the stopping parameters and triggers for the XW AGS (XW automatic generator starter)

Product Line:
XW AGS

Environment:
Determining all the stop trigger parameters

Cause:
Finding all the ways that AGS can automatically stop a generator

Resolution:

The AGS can automatically stop a generator in response to:
• Introduction of qualified grid power (grid power within acceptable parameters)
• High battery voltage • Battery charge stage (float or absorb stage)
• High battery SOC
• Removal of a high battery drain from the AC loads
• Thermostat signal
• Pre-programmed quiet time period.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings