Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do I adjust the battery temperature compensation using the system control panel?

Issue:
Adjusting the battery temperature compensation using the System Control Panel?

Product Line:
Conext XWXW+, Conext SW/SW+

Environment:
Installations that use either Conext SW/SW+ or Conext XW/XW+ with the System Control Panel

Cause:
Navigating through the System Control Panel to change the battery temperature compensation value.

Resolution:
Using the System Control Panel, you can start from the System Status and select the device, and enable the Advanced Settings

Note: If the Advanced Settings are not there; Press Enter, Up and Down.



Conext System Control Panel








Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings