Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What kind of generators use Type 9 in the AGS?
Issue:
Type of generators that use Type 9 in the AGS?

Product Line:
XW AGS, 865-1060

Environment:
Installations that have an Inverter/Charger(XW/XW+ or Conext SW)

Cause:
Types of generators that use type 9

Resolution:
Type 9 is a Start/Stop mode configuration.

Generators of this type are controlled with a three-position switch that is
normally in a center (or neutral) position. To start the generator, the
switch is pressed and held to the start position until the generator starts.
The switch is then released, and it returns to the center position. To stop
the generator, the switch is pressed and held to the stop position until the
generator stops. Again, releasing the switch returns it to the center
position.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings