Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Having issues using Configuration tool with Windows 8 or Windows 10
Issue:
Using the Configuration tool with Windows 8 or Windows 10, where it does not recognize the device and the device drivers.

Product Line:
XW Configuration tool, Conext Configuration tool

Environment:
Installations that use the configuration tool to perform upgrades or changes to the XW/XW+ or Conext SW series hybrid inverter/charger.

Cause:
When using Windows 8 or Windows 10, the computer does not recognize the configuration tool and its associated device driver

Resolution:
If using Windows 8 or Windows 10, you need to disable the driver signature first before uploading the device drivers.  You can do a google search or look in youtube and type in “Disabling driver signature for (Windows 8 or Windows 10).  Once you disable the driver signature you can then install the device driver and then the computer will recognize the configuration tool driver.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings