Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
​I don’t see the Equalize parameter on the Conext SW4024 using the System Control Panel?
Issue:
Equalize parameter

Product Line:
Conext SW hybrid inverter/charger

Environment:
Applications that use a system control panel and a Conext SW hybrid inverter/charger

Cause:
Applications that have issues accessing the equalize parameter

Resolution:
The Equalize parameter should be visible where it gives you the option to enable or disable it.  If you do not see it, check the battery type under charger settings.  If the Battery Type is set to Custom, and you can equalize your batteries, you need to enable equalize support under custom settings and then you can see the equalize parameter.
Note: When the system is set to Custom, as a safety precaution to make sure you are not equalizing the wrong set of batteries, you have to enable an additional parameter in order to equalize batteries.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings