Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
​The Configuration tool does not recognize the firmware file for single phase conversion XW+
Issue:
Software does not recognize the firmware file for single phase conversion

Product Line:
XW+/XW series hybrid inverter/charger

Environment:
Applications where a conversion is needed for the XW+5548 or XW6848

Cause:
If a firmware change is needed, the configuration software may not recognize the firmware file

Resolution:
Change the name of the file to a split phase firmware.

Example:
The file name for the single phase firmware file is 865-5548-2.02_03_00.BN0008.xf0.  The software will not recognize this file.  To resolve this, simply rename the file as if it was the split phase firmware which it would be 865-5548-01.02_03_00.BN0010.xf0

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings