Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
​How to perform charging test on a Conext XW/XW+ hybrid inverter/charger?
Issue:
Performing a charging test

Product Line:
XW+/XW hybrid inverter/charger

Environment:
Applications where the XW/XW+ are used

Cause:
How to perform a charging test

Resolution:

To perform the transfer and charger test:
1. Connect AC source to the inverter/charger.
2. Turn on the AC breaker (switch) to provide AC source to the inverter/charger.
3. The “Grid” or “Gen” LED on the information display panel should be flashing then turn to
solid upon qualifying AC.
4. Enable charge
5. Confirm the "Charging" LED on the information display panel is ON.
6. Verify the Bulk charge voltage climbs to within 56.6V~57.8Vdc (for XW6048, XW4548)
and 28.3~28.9Vdc (for XW4024), depend on the battery type.
7. Disable charge and turn off AC source.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings