Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where are the Xanbus connections in the MPPT60-150 controller

Issue:
MPPT Xanbus Communication

Product Line:
MPPT60-150 Solar Charge Controller

Environment:
Applications where an MPPT60-150 is used

Cause:
Location of communication ports

Resolution:

Xanbus is a network communications system developed by the manufacturer which allows the solar charge controller to communicate settings and activity to other Xanbus-enabled devices. Each Xanbus-enabled device is connected by a standard Ethernet (CAT 5/CAT 5e) patch cable.

See attached image.  The connections are inside the unit which would require opening the unit cover with the unit de energized.

Linked is an Instillation Guide for the device: Conext™ MPPT 60 Solar Charge Controller

Xanbus/Cat V port on device

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings