Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the separate ULSE sticker for panelboards?
Issue:
Separate ULSE sticker for panelboards Availability

Product Line:
Panelboards

Environment:
NQ, NF and I line panelboard

Cause:
Missing ULSE sticker

Resolution:
There is not a separate ULSE (UL Service entrance ) label that can be ordered for a panelboard like there is on a SWBD or MCC. There is a suitable for use as Service entrance label behind or on the back of the Panelboard deadfront. We ship this label on every panelboard regardless if it is factory assembled or if it is ordered from stock. The only difference is, a panel that is factory assembled with Service entrance selcted, will have the panel bonded at the factory to the green bonding screw.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings