Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a HCW12SN solid neutral, be installed into I line Combo panels ?
Issue:
Install a HCW12SN solid neutral into I line Combo panels

Product Line:
I Line Combo Panelboard Accessory

Environment:
Product Features

Cause:
Clarification

Resolution:
I line Combo panels use different solid neutrals than standard HCW, HCP, HCR I Line Panelboards
The use of I Line Panelboard neutrals mounted in I Line Combo panelboards is not recommended .

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings