Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can Circuit Breaker Panelboards Be Fed From the Side of the Box with Incoming Conductors?
Issue:
Can Circuit Breaker Panelboards Be Fed From the Side of the Box with Incoming Conductors?

Product Line:
Circuit Breaker panelboards sold and supported in the USA.

Environment:
Installation

Cause:
Installation

Resolution:
All of our circuit breaker panelboards are designed and tested for top or bottom entry.  Any other installation would be up to the local inspector for approval. We do not recommend it.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings