Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the torque value for the main incoming line lugs of all the MP Meter-Pak metering devices?
Cause:
Product Design Features

Product Line:
Meter-Pak™ Meter Centers

Resolution:
The torque value will depend on the catalog number of the Meter Pak device and the wire size used to supply the Meter Pak device.
The torque values for the Main Lugs for ALL Meter Pak devices can be found on the Labeling inside each Meter Pak device,
The labeling is applied to each device at the factory and is located on the back side of the customer compartment covers. This is the cover that goes over the complete tenant circuit breaker area.
The label will have a table showing each wire size and torque value.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings