Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a wire harness for the Masterpact cradle metering CT kits?
Issue:
Is there a wire harness for the Masterpact Cradle Metering CT kits?

Product Line:
Circuit Breakers

Resolution:
There is no wire harness included with, or available for, the Masterpact metering CT kits. The kit does include quantity (2) clips for help routing the wires, but the wiring must be supplied by the customer. The wire must follow the following specs:

Table showing specs required for wiring the metering CT kits

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings