Answer:
Issue:
Modbus protocol identification for a Conext Core XCNA
Product Line:
Conext Core XCNA inverters (XC540, XC630, XC680)
Environment:
Applications where Conext Core XCNA units are used
Cause:
Configuring the system correctly to comply with the Modbus protocols supported by the Conext Core XCNA
Resolution:
The Conext Core XC-NA series supports only the Modbus/RTU Protocol
NOTE: Modbus protocol supports RTU and ASCII protocols, but for the Conext Core XCNA it does not support ASCII protocols
Issue:
Modbus protocol identification for a Conext Core XCNA
Product Line:
Conext Core XCNA inverters (XC540, XC630, XC680)
Environment:
Applications where Conext Core XCNA units are used
Cause:
Configuring the system correctly to comply with the Modbus protocols supported by the Conext Core XCNA
Resolution:
The Conext Core XC-NA series supports only the Modbus/RTU Protocol
NOTE: Modbus protocol supports RTU and ASCII protocols, but for the Conext Core XCNA it does not support ASCII protocols
Released for: Schneider Electric USA